FRDM-K66F mbed serial&J-Link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-K66F mbed serial&J-Link

1,951 Views
penghaopenghao
Contributor II

我将刚拿到的FRDM-K66F开发板按FRDM-K66F|Freedom开发平台|Kinetis MCU|恩智浦

利用自带的micro-usb电缆接入PC(win7 32bit)后,安装mbedWinSerial_16466.exe,出现153126_153126.pngpastedImage_0.png。放弃。

然后,按照SEGGER - The Embedded Experts - OpenSDA / OpenSDA V2 里的顺序安装Setup_JLink_V510u.exe,先后试了4.68   5.02   5.10 5.12几个版本,也无法使板子被pc识别。153127_153127.pngpastedImage_5.png

如今项目非常紧。需要调试程序,而所有的下载调试工具,均不能正常使用,请提供帮助,谢谢

Labels (1)
0 Kudos
Reply
1 Reply

1,157 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

FRDM-K66 use OpenSDA v2.1 interface, please refer this document to see if it can help

Summary of FRDM-K22F debug interface

seem there is no P&E open sda firmware interface released yet, but you can refer Jlink and mbed parts.

Can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply