Error using Differential and Single-Ended ADC Channels in KDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error using Differential and Single-Ended ADC Channels in KDS

跳至解决方案
1,469 次查看
brycelembke
Contributor III

I have a need for both differential and single ended channels. When I use the ADC component from the component library and set some channels to be differential and some to be single-ended, I get the error 'Combining Differential and Single-Ended channel modes in A/D channel list required native result data format'. I have tried changing the Result Type, but I always get this error. Is there a way in KDS to use both Differential and Single-Ended channels on the same ADC? (My hardware is already spun, so it would be difficult to use the other ADC block).

I am using a K10DN512VLL10 with KDS 2.0.

 

Bryce

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
1,280 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Bryce,

In the "Result type" , please configure as this :

pastedImage_0.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,281 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Bryce,

In the "Result type" , please configure as this :

pastedImage_0.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,280 次查看
brycelembke
Contributor III

Perfect, that is what I needed.

0 项奖励
回复