Error in make(mcu on eclipse)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in make(mcu on eclipse)

3,199 Views
vigneshbalaji
Senior Contributor I

Hi,

    I am getting Error 2 in the console.I have attached the Screenshots also and the project also.

 

I followed Erich's post but I am not able to get it right https://mcuoneclipse.com/2013/07/21/diy-free-toolchain-for-kinetis-part-2-eclipse-ide/

Labels (1)
3 Replies

3,051 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

please download the project from GitHub here:

mcuoneclipse/Examples/Eclipse/FRDM-KL25Z/FRDM-KL25Z_Blink at master · ErichStyger/mcuoneclipse · Git...

How does it works with this project?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,051 Views
vigneshbalaji
Senior Contributor I

Hi Zhang,

               The project link which you have given is for KL25Z but I am using KEA-128. if you can provide me an example of KEA-128 on Eclipse IDE it will be great :smileyhappy:.

0 Kudos
Reply

3,051 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

the set of eclipse demo code was developed by Professor Erich Styger, the demo code is only available for K64/K25/K20/K60.

https://github.com/ErichStyger/mcuoneclipse/tree/master/Examples/Eclipse

user who uses other target please develop the code with referring those samples.

Hope this helps!

Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply