Does KDS support K02 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does KDS support K02 ?

1,301件の閲覧回数
davidchen-b3693
NXP Employee
NXP Employee

Hi team :

             Does KDS support K02 ? I didn't see it in device list when I create a new project . I found K02 sample code in KSDK update but it seems created with K22 . Does it is a official design rule create a K22 project for K02 device ? Thanks .

 

Best regards,

David

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,048件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello David:

The support for new devices in KDS is coming in the form of KSDK packages. In the next thread I attached a guide to install new packages:

MKL43Z supported?

:smileyalert: NOTE: The instructions are for KL43, just do the same but considering K02 instead.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信