Does KDS support K02 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does KDS support K02 ?

1,267 Views
davidchen-b3693
NXP Employee
NXP Employee

Hi team :

             Does KDS support K02 ? I didn't see it in device list when I create a new project . I found K02 sample code in KSDK update but it seems created with K22 . Does it is a official design rule create a K22 project for K02 device ? Thanks .

 

Best regards,

David

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,014 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello David:

The support for new devices in KDS is coming in the form of KSDK packages. In the next thread I attached a guide to install new packages:

MKL43Z supported?

:smileyalert: NOTE: The instructions are for KL43, just do the same but considering K02 instead.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply