Disable PEx Static Driver Warning

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Disable PEx Static Driver Warning

跳至解决方案
3,096 次查看
jasonphilippi
Contributor III

Hello,

 

I am looking to disable the following warning in my project (GPIO):

 

Warning: This value is not available on this decive but is configurable in static driver. (Digital Filter)

Processor Expert Problem.

 

 

I don't see a warning number of sorts to disable it.

I don't want to disable all warnings, how can I disable just this warning?

 

Thank you,

 

Jason

标签 (1)
0 项奖励
回复
1 解答
2,803 次查看
MarekTrmac
NXP Employee
NXP Employee

Jason,

I think the message means, that selected pin does not support the feature, even it is configurable in the API.

The Processor Expert warnings cannot be disabled. It is possible to configure content of the Problems view (in Provlems view drop down menu - Configure Content ...).

Regards,Marek

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,803 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Jason,

Which MCU are you using?

Could you tell post a screenshot of your workspace?

Thanks in advance!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 项奖励
回复
2,803 次查看
jasonphilippi
Contributor III

Hello Carlos,

I'm using KDS Version 3.0.0,  Processor Expert with KSDK 1.3 components, and a K24F .gpio-digital-filter.PNG

warnings.PNG

warning-settings.PNG

Let me know if you need any other relevant information.

Thank you,

Jason

0 项奖励
回复
2,804 次查看
MarekTrmac
NXP Employee
NXP Employee

Jason,

I think the message means, that selected pin does not support the feature, even it is configurable in the API.

The Processor Expert warnings cannot be disabled. It is possible to configure content of the Problems view (in Provlems view drop down menu - Configure Content ...).

Regards,Marek

0 项奖励
回复
2,803 次查看
jasonphilippi
Contributor III

Okay, this is what you are talking about, Help - Eclipse Platform.

  1. In Problems view, click the View Menu icon View Menu icon in the top right corner of the view.
  2. Use Configure Contents... to define your custom filter and click OK.
  3. In View Menu select Show and then your filter.

Thank you!

0 项奖励
回复