Demo eGUI(D4D) project for KDS.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Demo eGUI(D4D) project for KDS.

961件の閲覧回数
john71
Senior Contributor I

I've successfully compiled and run an eGUI demo project  for IAR. Now I'd like to run it on KDS. I'm struggling for two weeks to get it running - no luck. I include all needed files and configure peripherals - all as for the IAR project - and it compiles OK, without errors or warnings. But when I run, it eventually gets some exceptions and gets to Default Handler. I even can not to debug it - it's not traceable - can't see the cause of the problem in the debug perspective.

Can NXP team provide a working demo project for KDS? Is it so hard? Is it to much to ask?

ラベル(1)
0 件の賞賛
返信
0 返答(返信)