Debugging with built in debug interface of Freedom KL25Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugging with built in debug interface of Freedom KL25Z

Jump to solution
2,226 Views
avinashgupta
Contributor II

Hello,

 

I am just starting with KL25Z series. I have a Freedom KL25Z board which has OpenSDA debug adapter (http://www.pemicro.com/opensda/) is it supported by Kinetis Design Studio? Becasuse in document KDS200UG page 1 it says Kinetis Design Studio Supports

 

Support for SEGGER J-Link/J-Trace, P&E USB Multilink Universal/USB MultilinkUniversal FX andC MSIS-DAPdebugadapters

Labels (1)
1 Solution
2,187 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi,

yes, KDS can support OpenSDA. see

Kinetis Design Studio Integrated Development Envir|NXP

pastedImage_0.png

Can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,188 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi,

yes, KDS can support OpenSDA. see

Kinetis Design Studio Integrated Development Envir|NXP

pastedImage_0.png

Can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,187 Views
avinashgupta
Contributor II

Thanks.

Yes, just after posting this I figured out. I also successfully configured the debugger and also used it. All worked without any problem.

0 Kudos
Reply