Debugging with built in debug interface of Freedom KL25Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging with built in debug interface of Freedom KL25Z

ソリューションへジャンプ
2,197件の閲覧回数
avinashgupta
Contributor II

Hello,

 

I am just starting with KL25Z series. I have a Freedom KL25Z board which has OpenSDA debug adapter (http://www.pemicro.com/opensda/) is it supported by Kinetis Design Studio? Becasuse in document KDS200UG page 1 it says Kinetis Design Studio Supports

 

Support for SEGGER J-Link/J-Trace, P&E USB Multilink Universal/USB MultilinkUniversal FX andC MSIS-DAPdebugadapters

ラベル(1)
1 解決策
2,158件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi,

yes, KDS can support OpenSDA. see

Kinetis Design Studio Integrated Development Envir|NXP

pastedImage_0.png

Can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,159件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi,

yes, KDS can support OpenSDA. see

Kinetis Design Studio Integrated Development Envir|NXP

pastedImage_0.png

Can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,158件の閲覧回数
avinashgupta
Contributor II

Thanks.

Yes, just after posting this I figured out. I also successfully configured the debugger and also used it. All worked without any problem.

0 件の賞賛
返信