Hi Alice,
I attached images of the Debug configuration tabs and the error message received after I
clicked the debug icon.
So you see, everything compiles, but I can’t download the code.
I am using the TWR-KE18F board.
From the TWR-KE18F User’s guide document, page 6,
I believe that I need to get the board to load the demo code into flash and run in debug mode.
Thus, I believe that I have to get the board into CDSIS-DAP bootloader mode
and therefore I follow the instructions on document
TWR-KE18F User’s Guide, Rev. 0, 09/2015. page 6.,
I bring up the board by holding the reset button down while plugging in the USB cable
in order to get it into the bootloader mode.
David W. Potter
Senior Electrical Engineer
East Penn Manufacturing Co.
102 Deka Rd., Lyon Station, PA 19536
Ph. 610.682.6361 x3581
Automated Ph. 610.682.3150 x3581
dpotter@dekabatteries.com
http://www.dekabatteries.com