about MK22FN512's External bus clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about MK22FN512's External bus clock

1,271件の閲覧回数
andypeng
Contributor I

Hi,

   I use KSDK1.3.0 component library version set MK22FN512 clock system in KDS, found the external bus clock maximum is 30MHz, but if the kinetis component library version external bus clock maximum is 60MHz. this is what reason? I would like to work in KSDK1.3.0 component library version so that the external bus clock works at 60MHz, can you?

173866_173866.pngpastedImage_3.png

173865_173865.pngpastedImage_2.png

 

 

Thank you

Andy

ラベル(1)
0 件の賞賛
返信
1 返信

1,121件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Andy,

Please check the Reference Manual of MK22FN512VLL12,

the Maximum FlexBus clock(External bus clock) is 30MHZ.

pastedImage_1.png

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信