Debugger Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debugger Problem

1,925 次查看
michaelkoller
Contributor III

Hello!

 

When I try to debug any project, from one second to the other I get the error:

 

Error in final launch sequence

Failed to execute MI command:

-target-select remote localhost:3333

Error message from debugger back end:

localhost:3333: Connection timed out.

Failed to execute MI command:

-target-select remote localhost:3333

Error message from debugger back end:

localhost:3333: Connection timed out.

localhost:3333: Connection timed out.

 

I don't have a debugging session running (I think) and don't know how to fix this problem.

I would be glad if someone had a solution to this problem.Also, if you need more information, please ask!

 

Thanks and regards,

Michael

标签 (1)
0 项奖励
回复
2 回复数

1,554 次查看
michaelkoller
Contributor III

Thank you for the advice!

It worked again after i connected to the usb port, then reconnected it to the sda port again.

What I find strange is, that simply disconnecting and reconnecting it to the sda port as well as restarting the computer did not work.

But now it's ok, thanks again.

Best regards,

Michael

0 项奖励
回复

1,554 次查看
BlackNight
NXP Employee
NXP Employee

I would check for Zombies and use this check list:

https://mcuoneclipse.com/2014/11/03/debugging-failure-check-list-and-hints/

I hope this helps,

Erich

0 项奖励
回复