Debug issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug issue

1,740 Views
aaronmcdonald
Contributor I

Windows 10 has any one got this error message i can not debug my K64F in kinetis

Error in final launch sequence
Failed to execute MI command:
-target-select remote localhost:3333
Error message from debugger back end:
localhost:3333: The system tried to join a drive to a directory on a joined drive. I think its a driver issue please help

Labels (1)
0 Kudos
Reply
2 Replies

1,544 Views
BlackNight
NXP Employee
NXP Employee

Hello,

are you sure your board has still the debug (OpenSDA) firmware on it (see https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/ ) as there is a known issue with Windows 10?

Otherwise, can you check your debug settings (see https://mcuoneclipse.com/2016/04/13/fix-for-gdb-and-the-system-tried-to-join-a-drive-to-a-directory-... ).

I hope this helps,

Erich

0 Kudos
Reply

1,544 Views
aaronmcdonald
Contributor I

Hi

I am using Intelij as my ide.but i will try this thanks

0 Kudos
Reply