Crazy idea ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,643件の閲覧回数
piergiovannigor
Contributor II

NXP and Freescale will merge. Why not merge LPCxpresso and KDS saving the best of both worlds ?

Starting from LPCxpresso, Processor expert may be added as is .

Can KDSK included whit some work ?

Adding the PnE and other drivers may the system be working ?

LPCxpresso has a link2 driver whith j-link capabilities. Probably, apart from license problem it could be also used  for Freescale MCUs adding the live view of memory locations for M4 MCUs.

 

Thanks for your opinion.

 

Your Sincerely,

Pier Giovanni

ラベル(1)
0 件の賞賛
返信
1 解決策
3,270件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Pier Giovanni,

well, this is not a cracy idea. Both KDS and LPCXpresso are Eclipse based. KDS is stock Eclipse Luna with GNU ARM Embedded (launchpad) tools, while LPCXpresso comes with several extensions and additional features. Processor Expert itself is designed that it can be installed into any Eclipse, and this is already the case and used for different Eclipse distributions (Atollic TrueSTUDIO, Emprog ThunderBench).

With that said, you can use LPCXpressio with Processor Expert and the Kinetis SDK *today* :-). See this article for details.

As for the live view of memory locations: that might be indeed possible with the LPCXpresso debugger, but I have not tried that myself.

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,270件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello Pier Giovanni,

It is interesting idea to merge Processor Expert for Kinetis (par of the KDS) and LPCxpresso. I have tried slightly different configuration that described Erich in his blog post.

I have installed LPCxpresso v7.7.2 (LPCXpresso IDE Downloads | www.LPCware.com) and I have activated this installation as the Free Edition.

Because PEx for Kinetis (integrated in KDS) support GNU ARM Eclipse plugins I have installed these plugins by using Help > Install New Software... . I have used the http://gnuarmeclipse.sourceforge.net/updates link.

pastedImage_6.png

The LPCxpresso IDE is based on Eclipse Platform v4.4.2. Therefore I have downloaded and installed the

PEx-KINETIS-v3.0-PLUGIN-ECLIPSE_4.4 (REV 3.0.0) (see the page Processor Expert Software, Microcontroller Dr|Freescale):

pastedImage_2.png

Note:

The package contains freescale_updater.zip and PEx_for_Kinetis_3.0.0.zip. You need to install the Freescale updater firstly.

When you launch the LPCxpreso the default perspective is quite different. The Processor Expert windows are not visible. It can be added by using Processor Expert > Show Views command from the main menu. Windows are added and can be arranged.

A new Kinetis project can be created by using New Project Wizard (File > New > Kinetis Project).

I have created a new FRDM-K64F project without KSDK because KSDK has not been installed.

When I have set following Global Tool Path in Window > Preferences (see the screenshot below) I have been able to build the default project.

pastedImage_9.png

The LPCxpresso contains GBD SEGGER J-Link Debugging support by default. When you want to a P&E micro debugger (e.g. OpenSDA) you must install P&E micro GDB server driver for eclipse. You can use the Help > Install New Software... command and use the  http://www.pemicro.com/eclipse/updates link to install it directly.

When you open Debug Configurations windows you can add and select GDB P&E micro debug connection or GDB SEGGER J-link debug connetction:

pastedImage_13.png

Note:

The default configuration of GDB P&E Interface must be updated. There must be selected the Interface, Port, Device and updated the Executable path (default LPCxpresso path: ${cross_prefix}gdb${cross_suffix}), see the screenshot above.

The default LPCxpress installation does not contains any data about Freescale Kinetis derivatives. Therefore there is not possible to see any registers in the Debug perspective. You can install the EmbSysRegView plugins that are available at the http://embsysregview.sourceforge.net/update  site (use the Help > Install New Software... command).

When you start debugging, open the EmbSys Registers window (navigate to Window > Show View > Other and select the EmbSys Registers). In the EmbSys Registers window select SVD(CMSIS) architecture, Freescale vendor and the target Chip), see the screenshot below:

pastedImage_18.png

Summary:

The LPCxpresso Eclipse IDE can be used for installing Processor Expert for Kinetis, GNU ARM Eclipse plugins and other utilities. It seems that we are prepared for the merge.

Best Regards,

Marek Neuzil

0 件の賞賛
返信
3,270件の閲覧回数
piergiovannigor
Contributor II

Hi to all,

     the merged system seems to work fine.

I have problem to import files from KSDK, but this may be due to my knowledge since i have also trouble with KDS.

The file menu tab new links to Freescale devices, while new from "start here" window links to NXP devices. I think that someone whith the proper knowledge of Eclipse may change the menu file tab behviour to select both Freescale and NXP.

Just to end, the NXP Link2 probe ,obviously, does not have a selection for Freescale MCUs. The selection of generic M4 device does not work ( but also, the license is only for NXP devices).

Best Regards,

Pier Giovanni

0 件の賞賛
返信
3,270件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Pier Giovanni,

well, this is not a cracy idea. Both KDS and LPCXpresso are Eclipse based. KDS is stock Eclipse Luna with GNU ARM Embedded (launchpad) tools, while LPCXpresso comes with several extensions and additional features. Processor Expert itself is designed that it can be installed into any Eclipse, and this is already the case and used for different Eclipse distributions (Atollic TrueSTUDIO, Emprog ThunderBench).

With that said, you can use LPCXpressio with Processor Expert and the Kinetis SDK *today* :-). See this article for details.

As for the live view of memory locations: that might be indeed possible with the LPCXpresso debugger, but I have not tried that myself.

I hope this helps,

Erich

0 件の賞賛
返信
3,270件の閲覧回数
piergiovannigor
Contributor II

Hi Erich,

well, wonderfull, I will follow your article and I will try to degub a file on a n FRDM-K64F board using PnE, Segger SDA and

LPCxpresso debugger just to see what happen.

Yours Sincerely,

Pier Giovanni

0 件の賞賛
返信