Converting code to the KDS environment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Converting code to the KDS environment

ソリューションへジャンプ
1,663件の閲覧回数
rasa
Contributor I

Hi

 

I wrote a project in C on top of Ubunto which I need to run on top of the K64F, I already installed KDS 3.0.0 as well as KSDK 1.3.0 and the SEGGER J_LInk

1. Is there a automatic tool that can help me to do the conversion?

2. What are the steps I need to do in order to complete the task?

3. What are the necessary changes I need to do (e.g. printf)?

4. Is there is any good tutorial for the KDS?

 

Thanks in advance

ラベル(1)
0 件の賞賛
返信
1 解決策
1,598件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

I'm not aware of any document like that.

You can create a sample project with the wizard to be compliant with your hardware configuration.

The example will include all configuration to build and load the sample code on your board.

After that you can use this project and add your files.

On the community there are some posts explaining how to convert project from X dev tool (as CW for MCU V10.x) to KDS.

Under the KDS installation you can refer to the manuals (\KDS_3.0.0\doc)

  - KDS_Porting_Guide.pdf

  - KDS_Users_Guide.pdf

Under KSDK there are some documentations too under \KSDK_1.3.0\doc folder.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,599件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

I'm not aware of any document like that.

You can create a sample project with the wizard to be compliant with your hardware configuration.

The example will include all configuration to build and load the sample code on your board.

After that you can use this project and add your files.

On the community there are some posts explaining how to convert project from X dev tool (as CW for MCU V10.x) to KDS.

Under the KDS installation you can refer to the manuals (\KDS_3.0.0\doc)

  - KDS_Porting_Guide.pdf

  - KDS_Users_Guide.pdf

Under KSDK there are some documentations too under \KSDK_1.3.0\doc folder.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信