Converting Code Warrior10.6 project in KDS not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Converting Code Warrior10.6 project in KDS not working

1,641 Views
pallenna
Contributor II

Hi to Erich Styger,Adrian Sanchez Cano ,Tc Liew,jeremyzhou,Alice_Yang,

i am new to KDS IDE. i tried to importing a existing project from the Codewarrior 10.6 to KDS,and i followed the procedure of Importing MCU V10.6 projects (sample, using PE and MQX) under KDS, but it is not working. and i getting error as follows

make: *** [Test_TWR_K60DM100.elf] Error 1.

and i am sending the attachment please check it once,in this file if i did any mistakes please mention.

 

Thanks and Regards,

padmaja

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,367 Views
tsi-chung_liew
NXP Employee
NXP Employee

Pallenna,

Seems like the compiler path might not be selected. Go to C++ -> Tools -> option to configure it. Another method is to create a new project under KDS and use that as a reference.

Regards,

TsiChung

0 Kudos
Reply