Compile error using KDS - Interrupt/Exception

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Compile error using KDS - Interrupt/Exception

跳至解决方案
5,321 次查看
Donsnook
Contributor II

15:26:38 **** Incremental Build of configuration Debug for project Peak ****

make -k pre-build main-build

make: Interrupt/Exception caught (code = 0xc0000005, addr = 0x00411244)

 

15:26:39 Build Finished (took 170ms)

标签 (1)
1 解答
5,018 次查看
BlackNight
NXP Employee
NXP Employee

Hi Don,

can you check if you have any breakpoints or expressions/watchpoints set?

See http://mcuoneclipse.com/2014/10/11/failed-to-debug-with-gdb-breakpoints-or-expressions-on-non-existi...

I hope this helps,

Erich

在原帖中查看解决方案

8 回复数
5,018 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Don,

Please tell us your project in detailed ,  which chip ?  And  bareboard ? with PE ? SDK?

Then we can help you as soon as possible .

Best Regards

Alice

0 项奖励
回复
5,018 次查看
Donsnook
Contributor II

I'm using K22 freedom board, I have the USB setup as a CDC device, RTC enabled I'm working on setting up the SPI with DMA when I started seeing this. The first time I close SDK restarted was ok for a while. It starting happen again rebooted PC still had issues close out some other programs that I run on PC and was able to compile.

0 项奖励
回复
5,018 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Don,

Under the SDK, there is a "dspi_edma_demo" (C:\Freescale\KSDK_1.0.0\demos\dspi_edma_demo\kds), you can refer to this .

First run this demo on you board , then compare it with  your project .

Wish it helps you!
If you still have question, please contact me!

Alice

0 项奖励
回复
5,018 次查看
Donsnook
Contributor II

another strange issue unable to debug k22 freedom board or CDI hardware board base on K22 freedom

loading programming algorithm ...

  1. Done.

CMD>PM

  1. Programming.

Processing Object File Data ...

                               

.

  1. Programmed.

CMD>VC

Verifying object file CRC-16 to device ranges ...

   block 00000000-0000040F ...

  1. Ok.

   block 00000420-00019B0F ...

  1. Ok.

   Checksum Verification Successful. (Cumulative CRC-16=$AD31)

CMD>RE

  1. Initializing.

Target has been RESET and is active.

Disconnected from "127.0.0.1" via 127.0.0.1

Terminating Gracefully...

Target Disconnected.

0 项奖励
回复
5,019 次查看
BlackNight
NXP Employee
NXP Employee

Hi Don,

can you check if you have any breakpoints or expressions/watchpoints set?

See http://mcuoneclipse.com/2014/10/11/failed-to-debug-with-gdb-breakpoints-or-expressions-on-non-existi...

I hope this helps,

Erich

5,018 次查看
Donsnook
Contributor II

Erich,

I had break points but all were uncheck what I had to do is delete all break points

thanks

0 项奖励
回复
5,018 次查看
BlackNight
NXP Employee
NXP Employee

Yes, you have to delete them. Unchecking seems not be enough.

Erich

5,018 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Don,

Do you debug refer to the "kds_user_guide.pdf"-> 4.2 Debugging with the Kinetis Design Studio IDE   ? (C:\Freescale\KDS_1.1.1\doc\pdf)

If you still have question, please contact us!

Best Regards

Alice

0 项奖励
回复