Compile error using KDS - Interrupt/Exception

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compile error using KDS - Interrupt/Exception

ソリューションへジャンプ
5,252件の閲覧回数
Donsnook
Contributor II

15:26:38 **** Incremental Build of configuration Debug for project Peak ****

make -k pre-build main-build

make: Interrupt/Exception caught (code = 0xc0000005, addr = 0x00411244)

 

15:26:39 Build Finished (took 170ms)

ラベル(1)
1 解決策
4,949件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Don,

can you check if you have any breakpoints or expressions/watchpoints set?

See http://mcuoneclipse.com/2014/10/11/failed-to-debug-with-gdb-breakpoints-or-expressions-on-non-existi...

I hope this helps,

Erich

元の投稿で解決策を見る

8 返答(返信)
4,949件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Don,

Please tell us your project in detailed ,  which chip ?  And  bareboard ? with PE ? SDK?

Then we can help you as soon as possible .

Best Regards

Alice

0 件の賞賛
返信
4,949件の閲覧回数
Donsnook
Contributor II

I'm using K22 freedom board, I have the USB setup as a CDC device, RTC enabled I'm working on setting up the SPI with DMA when I started seeing this. The first time I close SDK restarted was ok for a while. It starting happen again rebooted PC still had issues close out some other programs that I run on PC and was able to compile.

0 件の賞賛
返信
4,949件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Don,

Under the SDK, there is a "dspi_edma_demo" (C:\Freescale\KSDK_1.0.0\demos\dspi_edma_demo\kds), you can refer to this .

First run this demo on you board , then compare it with  your project .

Wish it helps you!
If you still have question, please contact me!

Alice

0 件の賞賛
返信
4,949件の閲覧回数
Donsnook
Contributor II

another strange issue unable to debug k22 freedom board or CDI hardware board base on K22 freedom

loading programming algorithm ...

  1. Done.

CMD>PM

  1. Programming.

Processing Object File Data ...

                               

.

  1. Programmed.

CMD>VC

Verifying object file CRC-16 to device ranges ...

   block 00000000-0000040F ...

  1. Ok.

   block 00000420-00019B0F ...

  1. Ok.

   Checksum Verification Successful. (Cumulative CRC-16=$AD31)

CMD>RE

  1. Initializing.

Target has been RESET and is active.

Disconnected from "127.0.0.1" via 127.0.0.1

Terminating Gracefully...

Target Disconnected.

0 件の賞賛
返信
4,950件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Don,

can you check if you have any breakpoints or expressions/watchpoints set?

See http://mcuoneclipse.com/2014/10/11/failed-to-debug-with-gdb-breakpoints-or-expressions-on-non-existi...

I hope this helps,

Erich

4,949件の閲覧回数
Donsnook
Contributor II

Erich,

I had break points but all were uncheck what I had to do is delete all break points

thanks

0 件の賞賛
返信
4,949件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Yes, you have to delete them. Unchecking seems not be enough.

Erich

4,949件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Don,

Do you debug refer to the "kds_user_guide.pdf"-> 4.2 Debugging with the Kinetis Design Studio IDE   ? (C:\Freescale\KDS_1.1.1\doc\pdf)

If you still have question, please contact us!

Best Regards

Alice

0 件の賞賛
返信