CodeWarrier 10.6 link not available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrier 10.6 link not available

1,334 次查看
shishirbhosle
Contributor I

I am using KEA8 controller. I received CW 10.5 software but it dont have KEA8 controller libraries. On site it is given CodeWarrier 10.6 need to use but I dont get link to download it.

标签 (1)
0 项奖励
回复
1 回复

1,132 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Shishir

KEA family is supported from CodeWarrior v10.6.

The latest version is v10.6.6.

Please first install CW10.6.4 which can be downloaded from:

http://tinyurl.com/jjeggnz

Its update v10.6.5 and v10.6.6 are also available at the same link.

Further information and the release notes are available on the following Freescale community page:

https://community.freescale.com/docs/DOC-143655

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复