CodeWarrier 10.6 link not available

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrier 10.6 link not available

1,337件の閲覧回数
shishirbhosle
Contributor I

I am using KEA8 controller. I received CW 10.5 software but it dont have KEA8 controller libraries. On site it is given CodeWarrier 10.6 need to use but I dont get link to download it.

ラベル(1)
0 件の賞賛
返信
1 返信

1,135件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Shishir

KEA family is supported from CodeWarrior v10.6.

The latest version is v10.6.6.

Please first install CW10.6.4 which can be downloaded from:

http://tinyurl.com/jjeggnz

Its update v10.6.5 and v10.6.6 are also available at the same link.

Further information and the release notes are available on the following Freescale community page:

https://community.freescale.com/docs/DOC-143655

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信