Code example KV5x ADC in differential mode please

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code example KV5x ADC in differential mode please

1,916件の閲覧回数
winpennyjh
Contributor I


I need a code example of using the KV5x ADC in differential mode please.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,649件の閲覧回数
isaacavila
NXP Employee
NXP Employee

Hello Julian,

Kinetis KV5x series has 2 different ADC modules: 16-bit SAR ADC and 12-bit High Speed ADC (5MSPS).

For 16-bit SAR, this is the same module that is located in some Kinetis families, such as Kinetis 120MHz, with some little differences that are shown here: http://cache.nxp.com/files/microcontrollers/doc/app_note/AN5117.pdf?fpsp=1&WT_TYPE=Application%20Not... . These differences are  basically only one ADC instance, remove PGA module and other little differences in clock selection sources and trigger selection. You can use the Kinetis Migration Guide: K10 - 120 MHz to KV5x guide to migrate attached sample code that was created for K10_120MHz target. Sample code is reading ADC0_DP0 and ADC0_DM0 inputs in its basic configuration.

For HSADC module, There are no example codes for now (remember that KV5x part is still under preproduction stage). As soon as it gets ready for production, we can create sample codes for this module. Also, Kinetis SDK v2.0 is planned to support Kinetis V series family in mid July: Introducing Kinetis SDK v2.

For now, I hope this basic example code for 16-bit SAR configured in differential mode can be used as reference.

Regards,

Isaac

1,649件の閲覧回数
winpennyjh
Contributor I

Many thanks for the example code :smileyhappy:

0 件の賞賛
返信