Change target processor in KDS 3.2.0 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Change target processor in KDS 3.2.0 ?

跳至解决方案
1,552 次查看
blsousan
Contributor III

I am using the KDS 3.2.0 and currently have nice working project built using the processor expert based on the MKE202Z64VLC4.  I want to change it from this 64K Flash memory part to the MKE202Z16VLC4 version (which is the 16K variant).   However, I have not found a way to change it.  The two devices are the same with the exception of the 16K versus 64K one.   Is there a way to change it in the KDS?  (It would be time consuming to start all over again).

 

Thanks,

Bill

标签 (1)
0 项奖励
回复
1 解答
1,091 次查看
BlackNight
NXP Employee
NXP Employee

You can change the pinout in the CPU component like this: https://mcuoneclipse.com/2012/08/16/changing-the-cpu-with-processor-expert/  (description for ColdFire, but same applies to Kinetis/ARM).

Another one on this subject is here: https://mcuoneclipse.com/2016/06/25/switching-the-microcontroller-package-device-and-family/

I hope this helps,

Erich

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,092 次查看
BlackNight
NXP Employee
NXP Employee

You can change the pinout in the CPU component like this: https://mcuoneclipse.com/2012/08/16/changing-the-cpu-with-processor-expert/  (description for ColdFire, but same applies to Kinetis/ARM).

Another one on this subject is here: https://mcuoneclipse.com/2016/06/25/switching-the-microcontroller-package-device-and-family/

I hope this helps,

Erich

0 项奖励
回复