Can't Create Processor Expert Project for MK24FN1M0VLL12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't Create Processor Expert Project for MK24FN1M0VLL12

ソリューションへジャンプ
1,762件の閲覧回数
dmushow
Contributor I

I have made several attempts to create a processor expert project for the MK24FN1M0VLL12.  Every way I have tried results in the MK24FN1M0VLL12 being excluded from the drop down menu of processors available.  If I delete the processor from the project and attempt to add the exact processor I am interested in from the component library, the add feature fails to add anything to the project.  Below are pictures of the installed options and the project with the drop down list excluding the VLL12 processor.  Am I missing something? do I need to uninstall KDS and reinstall it?  Any help on the matter is greatly appreciated.

146924_146924.pngpastedImage_0.png

146925_146925.pngpastedImage_1.png

ラベル(1)
0 件の賞賛
返信
1 解決策
1,612件の閲覧回数
dmushow
Contributor I

I was finally able to get it working with the KSDK V 1.3 I created for the micro I am using and the New KSDK 1.X  or PE Project command.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,613件の閲覧回数
dmushow
Contributor I

I was finally able to get it working with the KSDK V 1.3 I created for the micro I am using and the New KSDK 1.X  or PE Project command.

0 件の賞賛
返信
1,612件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello David,

Can you use the KSDK+PE?

In the KSDK+PE project, there is the chip of MK24FN1M0VLL12:

pastedImage_0.png

I use KSDK1.3, i see you install KSDK1.2, i think the ksdk1.2 also have , if it not have , you can insatll

the version of KSDK1.3 .

Hope it helps

Alice

0 件の賞賛
返信