CPU Clock configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CPU Clock configuration

ソリューションへジャンプ
4,283件の閲覧回数
davidsherman
Senior Contributor I

Hello, I'm trying to configure the clock for a Kinetis MKE06Z128 on the FRDM-KE06 board.  I had an MQX-Lite application running using the default internal clock, but when I try to configure for the 8 MHz crystal, it doesn't work and the crystal is not oscillating.  Is there a separate component I need to add to control the OSC module?  I have these settings in the clock settings for the CPU module:

 

System Oscillator - checked

Clock Frequency - 8 MHz

Oscillator operating mode - low power

 

Clock source settings:

ICS mode - FEE

FLL output - 40 MHz (only option)

ICS output clock - 10 MHz (also tried 40 MHz, doesn't work)

 

I have enabled the SetClockConfiguration method under the CPU component.

ラベル(1)
0 件の賞賛
返信
1 解決策
3,023件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi David,

I have submitted a ticket (ENGR00317168) so hopefully this can be addressed.

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,023件の閲覧回数
davidsherman
Senior Contributor I

I've confirmed it, the code generated which configures the clocks has problems.  If I try to configure for FBE mode operation using an 8MHz crystal, the OSC_CR value it comes up with is 0x0, which is wrong, and the ICS_C1 value it comes up with is 0xC2, which is also wrong.  I'll try submitting a bug report, hopefully this will be fixed.

Edit:  I have found specifically what's wrong.  The CPU_Config.h that PE comes up with has the wrong values for CPU_ICS_C1_CONFIG_0, CPU_OSC_CR_CONFIG_0.  Not just a little wrong, but not even close.  Secondly, in CPU_Init.c, the initialization for CPU_ClockConfigDescriptors leaves out the initializer for OSC_CR_Value, so it will never populate the OSC_CR register properly.

If I try to configure the Kinetis for a 40 MHz core clock, 20 MHz bus clock, 40 MHz  running off an 8 MHz external crystal in FEE mode, the correct values should be:

OSC_CR = 0xB4 (Oscillator enabled, Oscillator enabled in stop mode, Oscillator clock source selected, Oscillator high range enabled, low power mode enabled)

ISC_C1 = 0x18 (FLL output selected as clock source, Reference divider = 256, external reference selected for FLL, Internal reference clock disabled)

ISC_C2 = 0x00 (Divide clock by 1)

If I try the same settings in PE, here is what it comes up with;

OSC_CR = 0x14 ( oscillator disabled,  oscillator clock source selected, oscillator high range enabled, low power mode enabled) - note that 0x0 is what actually gets written to OSC_CR.

ISC_C1 = 0x42 (Internal reference selected as clock source, reference divider = 32, external reference selected for FLL, Internal reference clock enabled)

ISC_C2 = 0x0 (divide clock by 1) - correct

0 件の賞賛
返信
3,024件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi David,

I have submitted a ticket (ENGR00317168) so hopefully this can be addressed.

Erich

0 件の賞賛
返信
3,023件の閲覧回数
ConstYu
NXP Employee
NXP Employee

Hi Eric,

I tried on my CW10.6, found the same issues, the problem is still remaining now. Can you help check whether this problem is fixed. Thanks. 

0 件の賞賛
返信
3,023件の閲覧回数
davidsherman
Senior Contributor I

Thanks Erich, I appreciate it.  I have submitted a ticket as well.  FYI, CodeWarrior 10.6 has the same problem.

0 件の賞賛
返信