'Build Project' has encountered a problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

'Build Project' has encountered a problem

2,174 Views
briancavanagh
Contributor III

Hi, this message never comes up when I'm at my office, only when I'm at home.

Known:

KDS Version 3.2.0

PE Micro Multilink Universal

MK22FN256VLH12

What I notice is at work when I choose 'Build Project', a file called 'EyeRelief.elf' is created.

I navigate to Debug Configurations and see 'EyeRelief.elf' at the location "C/C++ Application:" 

Before I leave work I copy the entire project file to my thumb drive. 

When I get on my home computer:

I drop the project on my desktop and I can still see EyeRelief.elf in the debug folder.

I then try to compile and I get the message below:

pastedImage_3.png

I then look in my debug folder and the EyeRelief.elf file is no longer there.

One attempt I tried to use to try and resolve this issue is:

Right-Click on Project Name, followed by 'Clean Project'.  I try and compile again with the same results.

Below are a couple of screen captures that I hope will provide some insight:

pastedImage_4.png

The capture above is what I see when I select "New_configuration" >> Main Tab

pastedImage_5.png

The capture above is what I see when I select "New_configuration" >> Debugger Tab

Can someone give me some guidance on how to correct this?

Thanks,

Brian

0 Kudos
Reply
1 Reply

1,929 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Brian,

From your description, there is problem when you build ,

I think maybe after you copy the project, the path has some error , please check it .

Or you can also share it , I help you check it on my side .

If the project is private , you can also submit a service request on NXP to send it :

How to submit a new question for NXP Support 

 

Hope it helps

Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply