Always display program size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Always display program size

ソリューションへジャンプ
2,338件の閲覧回数
remibeges
NXP Employee
NXP Employee

My program size will it seems overflow heap memory (KL26Z128)

 

c:/freescale/kds_3.0.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/bin/ld.exe: FSFK_KL26Z.elf section `._user_heap_stack' will not fit in region `m_data' c:/freescale/kds_3.0.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/bin/ld.exe: region `m_data' overflowed by 508 bytes

 

I tried modifying in DebugConfiguration the target platform to KL26Z256 to trick the linker in order to print size, but this does not seem to have any impact. I looked at the linker file, and it is still the one for KL26Z128, not 256

 

/* ################################################################### */

/*##

/*##     This component module is generated by Processor Expert. Do not modify it. */

/*##                                   */

/*##     Filename  : ProcessorExpert.ld */

/*##                                   */

/*##     Project   : FSFK_KL26Z        */

/*##                                   */

/*##     Processor : MKL26Z128VLH4     */

/*##                                   */

/*##     Compiler  : GNU C Compiler    */

/*##                                   */

/*##     Date/Time : 2015-08-18, 14:51, # CodeGen: 41 */

/*##                                   */

/*##     Abstract  :                   */

/*##                                   */

/*##     This file is used by the linker. It describes files to be linked, */

/*##     memory ranges, stack size, etc. For detailed description about linker */

/*##     command files see compiler documentation. This file is generated by default. */

/*##     You can switch off generation by setting the property "Generate linker file = no" */

/*##     in the "Build options" tab of the CPU component and then modify this file as needed. */

/*##

/*##                                   */

/*## ###################################################################*/

 

 

 

 

/* Entry Point */

ENTRY(__boot)

 

 

/* Highest address of the user mode stack */

_estack = 0x20003000;    /* end of m_data */

__SP_INIT = _estack;

__stack = _estack;

 

 

/* Generate a link error if heap and stack don't fit into RAM */

__heap_size = 0x00;                    /* required amount of heap  */

__stack_size = 0x0400;                 /* required amount of stack */

 

 

MEMORY {

  m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x000000C0

  m_text      (RX) : ORIGIN = 0x00000410, LENGTH = 0x0001FBF0

  m_data      (RW) : ORIGIN = 0x1FFFF000, LENGTH = 0x00004000

  m_cfmprotrom  (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010

}

How can I change the linker configuration so it can complete the linking and size of the program can then be printed ?

Then, which optimizations can I make to reduce heap memory consumption ?

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
2,133件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Increase in the MEMORY block the LENGTH for m_text and m_data?

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,133件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Increase in the MEMORY block the LENGTH for m_text and m_data?

Erich

0 件の賞賛
返信
2,133件の閲覧回数
remibeges
NXP Employee
NXP Employee

Hi Erich, Indeed that worked, thanks. Sometimes things are so obvious :smileysilly:

0 件の賞賛
返信