Mcuxpresso Crashes while debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mcuxpresso Crashes while debugging

1,438 Views
giane
Contributor I

Hello,

I am building an application on a MKS20FN256VLH12 mcu and I face frequent crashes than ever when debugging. I have read the "knownIssues.txt" when I downloaded the latest Mcuxpresso version (MCUXpresso IDE v11.8.0 [Build 1165] [2023-07-26]) and there's a part that says something about a "slow debug start if the global variables view is open and there are a lot of var inside the elf". I have tried hiding that tab and opening whenever I needed it but somehow the program still crashes a lot. I will attach the log and from what I have seen it says something about not finding the address of a variable I was watching.

I would greatly appreciate some help since it is very annoying to constantly re-open the program

Here are some specs:

OS = Windows 11

Mcuxpresso Version = MCUXpresso IDE v11.8.0 [Build 1165] [2023-07-26]

SDK Used = SDK_2.x_MKS20FN256xxx12

Mcuxpresso last session log: https://hastebin.com/share/odeqopisur.yaml

0 Kudos
Reply
0 Replies