TJA1043 application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1043 application

Jump to solution
3,743 Views
loswe
Contributor II

你好,对于TJA1043的应用原理图(page 19)我有个疑问想请教:

TJA1043的INH引脚控制了给TJA1043的VCC引脚供电的5V电源芯片的使能引脚,那么当INH拉低5V电源芯片的使能引脚,5V电源芯片不能给TJA1043的VCC引脚供电,TJA1043没有供电,它如何输出INH信号来拉高5V电源芯片的使能呢

0 Kudos
Reply
1 Solution
3,706 Views
guoweisun
NXP TechSupport
NXP TechSupport
6 Replies
3,737 Views
guoweisun
NXP TechSupport
NXP TechSupport

 

INH 是上拉到VBAT的,通过外部设置STB/EN来控制TJA1043的状态控制INH的H/L,他是一直受控的因为VBAT没断电,比方说上电VBAT以后 TJA1043工作在sleep的模式,STB/EN都是floating的无法唤醒他,那么可以通过本地wake pin 或者Remote wake-up (via the CAN bus)唤醒 让INH 拉高从而让TJA1043 工作:

Any wake-up request, setting the Pwon flag or a LOW-to-HIGH transition on STB_N will
clear UVNOM and the timers, allowing the voltage regulators to be reactivated (at least until
UVNOM is set again).

guoweisun_0-1753941245889.pngguoweisun_1-1753941263720.png

 

3,731 Views
loswe
Contributor II

常电应用场景中VBAT是不断电的,按照参考应用原理图,本地wake pin是通过电阻上拉到VBAT的,那wake pin始终是高电平,是不是就不能用来控制唤醒。

via the CAN bus的话,TJA1043的VCC没有供电,它可以收到CAN bus的唤醒报文吗。

0 Kudos
Reply
3,719 Views
guoweisun
NXP TechSupport
NXP TechSupport

Sleep 模式VCC本来就没电了

您仔细看看AH1014 page45:6.2.4 Sleep Mode 

Application Hints

0 Kudos
Reply
3,710 Views
loswe
Contributor II

您给的资料中提到了While the microcontroller is completely un-powered (no VCC supply),
the TJA1043 keeps partly alive via its battery supply. It allows the transceiver to monitor
the bus for CAN messages。我理解这就是TJA1043可以在没有VCC的情况下继续监听总线报文的原因吧

0 Kudos
Reply
3,706 Views
guoweisun
NXP TechSupport
NXP TechSupport

对的

 

3,703 Views
loswe
Contributor II
谢谢
0 Kudos
Reply