I keep getting a GPS compass inconsistent error.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I keep getting a GPS compass inconsistent error.

ソリューションへジャンプ
3,059件の閲覧回数
nxf58541
NXP Employee
NXP Employee

After a second crash of my drone, I kept getting GPS compass inconsistent messages when trying to arm the drone. Using the mavlink console, I saw that there were 2 mag sensors listed, with the sensor # 0 being listed as the primary. To fix the problem temporarily, I simply disabled mag sensor # 1 using the Parameter modifications. So, can someone tell me why sensor # 1 would be off from sensor # 0? Where is sensor # 1 vs. sensor # 0? Is it OK to fly with sensor # 1 disabled? Is there a way to recalibrate sensor # 1 or somehow "reset" sensor # 1?

0 件の賞賛
返信
1 解決策
3,034件の閲覧回数
nxf58541
NXP Employee
NXP Employee

We don't have a root cause of why the sensors are off, but they are. This is partially PX4 issue as at one point they made this too sensitive. Most people just disable the mag on the FMU and use the one on the compass.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,035件の閲覧回数
nxf58541
NXP Employee
NXP Employee

We don't have a root cause of why the sensors are off, but they are. This is partially PX4 issue as at one point they made this too sensitive. Most people just disable the mag on the FMU and use the one on the compass.

0 件の賞賛
返信