I keep getting a GPS compass inconsistent error.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I keep getting a GPS compass inconsistent error.

跳至解决方案
3,068 次查看
nxf58541
NXP Employee
NXP Employee

After a second crash of my drone, I kept getting GPS compass inconsistent messages when trying to arm the drone. Using the mavlink console, I saw that there were 2 mag sensors listed, with the sensor # 0 being listed as the primary. To fix the problem temporarily, I simply disabled mag sensor # 1 using the Parameter modifications. So, can someone tell me why sensor # 1 would be off from sensor # 0? Where is sensor # 1 vs. sensor # 0? Is it OK to fly with sensor # 1 disabled? Is there a way to recalibrate sensor # 1 or somehow "reset" sensor # 1?

0 项奖励
回复
1 解答
3,043 次查看
nxf58541
NXP Employee
NXP Employee

We don't have a root cause of why the sensors are off, but they are. This is partially PX4 issue as at one point they made this too sensitive. Most people just disable the mag on the FMU and use the one on the compass.

在原帖中查看解决方案

0 项奖励
回复
1 回复
3,044 次查看
nxf58541
NXP Employee
NXP Employee

We don't have a root cause of why the sensors are off, but they are. This is partially PX4 issue as at one point they made this too sensitive. Most people just disable the mag on the FMU and use the one on the compass.

0 项奖励
回复