pca9685 pwm frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pca9685 pwm frequency

4,143 Views
longzhengbing202002
Contributor II

The maximum PWM frequency of PCA9685 is 1500Hz. Can this maximum frequency be increased to 3000Hz? Or is there an alternative IC with a maximum PWM frequency of 3000Hz? Thank you.

0 Kudos
Reply
11 Replies

4,130 Views
longzhengbing202002
Contributor II
How should I operate if I need a PWM frequency of 3000 Hz?
0 Kudos
Reply

4,127 Views
guoweisun
NXP TechSupport
NXP TechSupport

选择这个吧---PCA9956

0 Kudos
Reply

4,122 Views
longzhengbing202002
Contributor II
如果PCA9685 通过外接50MHZ的输入 能改变输出频率加倍是最好的 我可以直接替换
0 Kudos
Reply

4,034 Views
guoweisun
NXP TechSupport
NXP TechSupport

这样使用应该不可以

0 Kudos
Reply

4,028 Views
longzhengbing202002
Contributor II

从这个时钟图来看。这个外部时钟输入没有经过分频。进入与内部时钟的选通器。这个时钟源频率加倍。输出的pwm频率也应该加倍吧

0 Kudos
Reply

4,021 Views
guoweisun
NXP TechSupport
NXP TechSupport

guoweisun_0-1746510344212.png

 

你可以测试下按照上面的这个公式。

0 Kudos
Reply

3,370 Views
longzhengbing202002
Contributor II

通过测试验证 外接50M 晶振⑧分频系数设置为3 可以把频率提高到3000hz

0 Kudos
Reply

4,124 Views
longzhengbing202002
Contributor II
这个频率不能调节 需要频率可调
0 Kudos
Reply

4,120 Views
guoweisun
NXP TechSupport
NXP TechSupport

你是要具体怎么使用?为何非要用3KHZ的频率?

0 Kudos
Reply

4,116 Views
longzhengbing202002
Contributor II
原来的1.5kHZ 在我们的摄像头光源上 会有点干扰 我们想把频率提高一倍
0 Kudos
Reply

4,106 Views
guoweisun
NXP TechSupport
NXP TechSupport

没有更合适的产品可以推荐目前,建议确认是不是这个频率端引起的,可以通过操作PRE_SCALE寄存器去更改频率试试。

0 Kudos
Reply