NVT4858 for QSPI voltage level translation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NVT4858 for QSPI voltage level translation

1,150件の閲覧回数
vjen
Contributor I

The NVT4858 is designed for SD and SIM application. Can I use it for QPSI?

My circuit:

Host side: 1.2V QSPI, SCLK is up to 50 MHz

Flash memory: 3.3V QSPI

Please advise. Thanks.

ラベル(2)
0 件の賞賛
返信
1 返信

1,139件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Vance,

please refer to the NVT4858 datasheet. Yes, the NVT4858 fulfills your requirements. 

The NVT4858 is designed for SD and SIM application. Can I use it for QPSI?

JozefKozon_0-1748321478169.png

Host side: 1.2V QSPI, SCLK is up to 50 MHz

JozefKozon_1-1748321553242.pngJozefKozon_2-1748321581043.png

Flash memory: 3.3V QSPI

JozefKozon_3-1748321614567.png

With Best Regards,

Jozef