PCA85133U/2DA/Q1Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA85133U/2DA/Q1Z

Jump to solution
1,401 Views
ppnachi
Contributor I

Hi,

My Segment LCDs are in production from China. To choose a driver IC for the LCDs, I found a NXP part number PCA85133U/2DA/Q1Z.  

 

This is a bare die chip. According to the datasheet it says this chip is compatible for COG fabrication. But for my application, I'm looking for a COB bare die chip. 

 

My question is does the above mentioned part number will support for the COB fabrication? If yes I want to buy bulk quantity. 

 

Waiting for your reply and advise 

Rgds 

Nazar PP 

 

0 Kudos
Reply
1 Solution
1,375 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The PCA85133U/2DA/Q1Z is a bare die chip optimized for anisotropic conductive film (ACF) bonding. 
 
As the COB fabrication typically requires a packaged IC or a bare die with suitable wire bonding and encapsulation support for mounting on a PCB, the PCA85133U/2DA/Q1Z is not suitable for that.
 
BRs, Tomas

View solution in original post

0 Kudos
Reply
1 Reply
1,376 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The PCA85133U/2DA/Q1Z is a bare die chip optimized for anisotropic conductive film (ACF) bonding. 
 
As the COB fabrication typically requires a packaged IC or a bare die with suitable wire bonding and encapsulation support for mounting on a PCB, the PCA85133U/2DA/Q1Z is not suitable for that.
 
BRs, Tomas
0 Kudos
Reply