EIS BMS reference software source code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EIS BMS reference software source code

256 Views
gferretts
Contributor II

To evaluate and develop a EIS bms we bought an evaluation board with BCC 7426 (EVBMA7X2YDT1).

The problem is that the only reference software i found on NXP package manager is precompiled "SW32K358_EIS_BMU_SW_3.0_CD01_D2605" to be used in combination with "SW32K358_EIS_GUI_SW_3.0_CD01_D2605".

The release documentation explain how to use the GUI with S32K358_EIS_BMU board flashing the provided .elf. Is it possible to download the source code of reference software source code, in order to use the GUI with a compatible board (RD-BESSK358BMU) which has quite the same layout (K358 with MC33665A, 2 TPL ports, Debug Header) but different pinout on SPI and UART? Seems strange it has been changed from one board to other one.

Thanks

Tags (5)
0 Kudos
Reply
1 Reply

158 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi gferretts

The currently released SW32K358_EIS_BMU_SW_3.0_CD01_D2605 software package primarily provides pre-compiled BMU firmware along with the corresponding EIS GUI.

Based on the existing release content, No any publicly downloadable complete source code for the BMU reference software.

0 Kudos
Reply