Analog Front End Layout

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Analog Front End Layout

269 Views
s1hukla
Contributor I

I am designing a PCB based around a TI CC1310. I plan to operate it around 915 MHz with an SMA connected whip antenna. Ideally, I would like to get 4-5 kilometers line-of-sight range at 50 kbs or lower, which seems doable if I have a decent RF frontend. However, RF is definitely not my expertise, so my plan was just to copy the CC1310 balun and filter layout as closely as possible. Unfortunately, that's going to be more complicated and expensive than I had anticipated, so I'm wondering how much wiggle room I have when it comes to layout before I totally destroy my performance.

In particular, TI used a stack-up that is 0.175 mm between the ground and top signal plane. I can save some money if I extend that to 0.21 mm, which I don't think will affect performance much, but I'm not sure. I can also save some effort by swapping out some of the passive components with those from another company, but I'm not sure how risky that is. I noticed that even the same part numbers have different footprints than what were used on the TI board. I assume that won't affect too much though. Finally, I would like to shorten the trace between the end of the filter and the antenna connector/blocking capacitor, which I assume won't affect much as long as I keep it 50 Ohms.

Assuming I keep the components pretty close together and the layout symmetrical, how much can I alter the layout before I have to worry about performance being degraded? Should I plan on having to select new frontend components if I make any of the changes mentioned?

Labels (1)
0 Kudos
Reply
1 Reply

242 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi s1hukla

What can I do for your about NXP products support!

Thanks!

 

 

0 Kudos
Reply