guider can't edit code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

guider can't edit code

1,584 Views
susan1999
Contributor I

Hello

i'm using 1.5.0, fond some question:

1.image no rotate animation,and rotation center offset;

2.code viewer only for view,can't edit code, this is a significant flaw.

becauce if want to click a button another image move or rotate.GUIder unable to achieve.

so the two button functions should be modified:

[Generate Code] only generate code;

[Simulator] only build and run (do not generate);

then,i can generate code if i need, or i can edit code to do some thing that GUIder not achieved;

I hope to do everything well in the GUIder and see the simulation run,then migrate to other devices.

  

Best regards

0 Kudos
Reply
1 Reply

1,565 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @susan1999 

Thanks so much for your suggestions, I will forward them to development team, thanks!

 

BR

Alice

0 Kudos
Reply