Why is The device not connected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why is The device not connected

Jump to solution
1,642 Views
dsd
Contributor I

The gui guider fails to connect to the LPC5506.via jlink

0 Kudos
Reply
1 Solution
1,619 Views
nxa22510
NXP Employee
NXP Employee

Could I double confirm with as you what's the board you're using? If the board was LPC5506 you used, it's not supported and we didn't test in the previous releases. But the board of LPC55S06 supported. You will find the list of  supported boards in the documents and also could see the detailed supported boards when you creating the project.

View solution in original post

0 Kudos
Reply
1 Reply
1,620 Views
nxa22510
NXP Employee
NXP Employee

Could I double confirm with as you what's the board you're using? If the board was LPC5506 you used, it's not supported and we didn't test in the previous releases. But the board of LPC55S06 supported. You will find the list of  supported boards in the documents and also could see the detailed supported boards when you creating the project.

0 Kudos
Reply