Why is The device not connected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why is The device not connected

ソリューションへジャンプ
2,254件の閲覧回数
dsd
Contributor I

The gui guider fails to connect to the LPC5506.via jlink

0 件の賞賛
返信
1 解決策
2,231件の閲覧回数
nxa22510
NXP Employee
NXP Employee

Could I double confirm with as you what's the board you're using? If the board was LPC5506 you used, it's not supported and we didn't test in the previous releases. But the board of LPC55S06 supported. You will find the list of  supported boards in the documents and also could see the detailed supported boards when you creating the project.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,232件の閲覧回数
nxa22510
NXP Employee
NXP Employee

Could I double confirm with as you what's the board you're using? If the board was LPC5506 you used, it's not supported and we didn't test in the previous releases. But the board of LPC55S06 supported. You will find the list of  supported boards in the documents and also could see the detailed supported boards when you creating the project.

0 件の賞賛
返信