Spinbox Widget with no decimal digits causes rendering issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Spinbox Widget with no decimal digits causes rendering issues

1,839件の閲覧回数
mitchkapa
Contributor III

GUI Guider 1.4.0 -> LVGL v8.2.0 -> LPC54S018

Within GUI Guider creating a Spinbox Widget that has 0 digits after the decimal place seems to cause a rendering issue that affects most of the items within that screen.  Objects disappear and then will usually reappear if selected from the screen menu on the left side.  But the Spinbox Widget itself also renders incorrectly (see screenshot below).

I think this only impacts working within GUI Guider.  Once the code is actually running the objects display correctly.  At least with the Simulator (C) I haven't verified on hardware yet.

mitchkapa_0-1660168564201.pngmitchkapa_0-1660168564201.png

 

 

0 件の賞賛
返信
1 返信

1,816件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello mitchkapa,

Yes, I have check it on my side, the same with you, there's at least one digits after the decimal place .

I will report it to development team, thanks!

 

BR

Alice

0 件の賞賛
返信