LEDs appear as a mostly white circle with GUI Guider 1.4.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LEDs appear as a mostly white circle with GUI Guider 1.4.0

2,482 Views
mitchkapa
Contributor III

With GUI Guider 1.4.0 I am finding that the LED appears as a mostly white circle surrounded by a ring of whatever the selected LED color was.  In addition the Attributes tab for the LED is missing the ability to turn the LED ON or OFF.

In addition to this apparent bug if controlling the LED ON/OFF through the Event tab was an option I think that would be a nice feature.

0 Kudos
Reply
3 Replies

2,466 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  mitchkapa,

 

Could you please take a video or screenshot show the issue? And tell us which chip you use?

 

BR

Alice

0 Kudos
Reply

2,462 Views
mitchkapa
Contributor III

I am using GUI Guider 1.4.0 -> LVGL v8.2.0 -> LPC54S018

Here is a screenshot of what I see for an LED on the Simulator (C).  The behavior is the same running on the actual hardware.

mitchkapa_0-1660050026234.png

 

0 Kudos
Reply

2,428 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Thanks for your sharing, I will check on my side and report it to development team after confirm. 

 

BR

Alice

0 Kudos
Reply