Spinbox Widget with no decimal digits causes rendering issues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Spinbox Widget with no decimal digits causes rendering issues

1,430 次查看
mitchkapa
Contributor III

GUI Guider 1.4.0 -> LVGL v8.2.0 -> LPC54S018

Within GUI Guider creating a Spinbox Widget that has 0 digits after the decimal place seems to cause a rendering issue that affects most of the items within that screen.  Objects disappear and then will usually reappear if selected from the screen menu on the left side.  But the Spinbox Widget itself also renders incorrectly (see screenshot below).

I think this only impacts working within GUI Guider.  Once the code is actually running the objects display correctly.  At least with the Simulator (C) I haven't verified on hardware yet.

mitchkapa_0-1660168564201.png

 

 

0 项奖励
回复
1 回复

1,407 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello mitchkapa,

Yes, I have check it on my side, the same with you, there's at least one digits after the decimal place .

I will report it to development team, thanks!

 

BR

Alice

0 项奖励
回复