How to use GUI_guider V1.2 build file system support hmi project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to use GUI_guider V1.2 build file system support hmi project

跳至解决方案
4,587 次查看
ClusterDesign
Contributor I

Dear Support:

    Recently we use GUI_Guider V1.2 building HMI project based on RT1170 EVK board. Unfortunately, i can not find the file system supporting settings on that tool. Each picture generate a .c source code. That's impossible for us to use this tool to create a project with nearly 1000 pictures in .c code. I wish to know how can i use GUI_guider to create a HMI project can split picture & font using file system to store the file in flash or eMMC not using .c files. 

0 项奖励
回复
1 解答
4,568 次查看
zhenhualuo
NXP Employee
NXP Employee

Hi, 

Currently GUI Guider doesn't support settings to load fonts and images from external storage (e.g. eMMC), this is a new feature planned in future release. LVGL library supports file system module and loading images from external storage, can you please check if the following guide could help? 

https://docs.lvgl.io/7.11/overview/image.html 

https://docs.lvgl.io/7.11/overview/file-system.html

Best Regards, 

Zhenhua 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,569 次查看
zhenhualuo
NXP Employee
NXP Employee

Hi, 

Currently GUI Guider doesn't support settings to load fonts and images from external storage (e.g. eMMC), this is a new feature planned in future release. LVGL library supports file system module and loading images from external storage, can you please check if the following guide could help? 

https://docs.lvgl.io/7.11/overview/image.html 

https://docs.lvgl.io/7.11/overview/file-system.html

Best Regards, 

Zhenhua 

0 项奖励
回复
4,542 次查看
ClusterDesign
Contributor I

Hi Zhenghua:

  Thanks for your reply, i wait in hope the version GUI_Guider in future release support file system. So that can expand the tool usage in HMI products.

0 项奖励
回复