How to use GUI_guider V1.2 build file system support hmi project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use GUI_guider V1.2 build file system support hmi project

Jump to solution
4,539 Views
ClusterDesign
Contributor I

Dear Support:

    Recently we use GUI_Guider V1.2 building HMI project based on RT1170 EVK board. Unfortunately, i can not find the file system supporting settings on that tool. Each picture generate a .c source code. That's impossible for us to use this tool to create a project with nearly 1000 pictures in .c code. I wish to know how can i use GUI_guider to create a HMI project can split picture & font using file system to store the file in flash or eMMC not using .c files. 

0 Kudos
Reply
1 Solution
4,520 Views
zhenhualuo
NXP Employee
NXP Employee

Hi, 

Currently GUI Guider doesn't support settings to load fonts and images from external storage (e.g. eMMC), this is a new feature planned in future release. LVGL library supports file system module and loading images from external storage, can you please check if the following guide could help? 

https://docs.lvgl.io/7.11/overview/image.html 

https://docs.lvgl.io/7.11/overview/file-system.html

Best Regards, 

Zhenhua 

View solution in original post

0 Kudos
Reply
2 Replies
4,521 Views
zhenhualuo
NXP Employee
NXP Employee

Hi, 

Currently GUI Guider doesn't support settings to load fonts and images from external storage (e.g. eMMC), this is a new feature planned in future release. LVGL library supports file system module and loading images from external storage, can you please check if the following guide could help? 

https://docs.lvgl.io/7.11/overview/image.html 

https://docs.lvgl.io/7.11/overview/file-system.html

Best Regards, 

Zhenhua 

0 Kudos
Reply
4,494 Views
ClusterDesign
Contributor I

Hi Zhenghua:

  Thanks for your reply, i wait in hope the version GUI_Guider in future release support file system. So that can expand the tool usage in HMI products.

0 Kudos
Reply