How to display multi-language on the screen with LVGL using Gui Guider?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to display multi-language on the screen with LVGL using Gui Guider?

跳至解决方案
3,932 次查看
ChesterLee
Contributor II

Now I'm going to develop a product with displaying multi-language (such as Chinese, English, Russian, etc.) on the LCD screen using LVGL. I wonder if there is a way to set widgets' texts with parameters? Like define a series of parameters about language and use them set text content:

/* --------------------------- Code example --------------------------- */

typedef struct {

    char *itemChinese,

    char *itemEnglish,

} param_language_t;

param_language_t param_language = {

    .itemChinese = "你好",

    .itemEnglish = "Hello",

};

lv_label_set_text_fmt(ui->screen_main_label_hello, "%s", param_language.itemEnglish);

/* --------------------------- Code example --------------------------- */

Or just using a middleware named lv_i18n, which also needs using parameters to set widgets text.

标记 (2)
0 项奖励
回复
1 解答
3,899 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @ChesterLee ,

Thanks for your post. According to GUI Guider v1.8.1 User Guide, currently the GUI Guider IDE only supports two language: English and Chinese. However, this can be achieved by developing custom code. The following is an example.

Celeste_Liu_0-1731562555570.png

For the detailed description of this example, you can refer to the section of "7.10 How to develop a multi - language application".

Celeste_Liu_1-1731563390966.png

Hope it helps.

Best Regards,

Celeste

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,900 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @ChesterLee ,

Thanks for your post. According to GUI Guider v1.8.1 User Guide, currently the GUI Guider IDE only supports two language: English and Chinese. However, this can be achieved by developing custom code. The following is an example.

Celeste_Liu_0-1731562555570.png

For the detailed description of this example, you can refer to the section of "7.10 How to develop a multi - language application".

Celeste_Liu_1-1731563390966.png

Hope it helps.

Best Regards,

Celeste

0 项奖励
回复
3,895 次查看
ChesterLee
Contributor II

Hi @Celeste_Liu ,

Tks for your kindly reply. I wish Gui Guider could support more languages in the future. Anyway, tks a lot!

Best Regard

Chester

0 项奖励
回复
3,876 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @ChesterLee ,

I'm glad to help you. I will feed back your suggestion. Any new issues, welcome to create a new thread.

BRs,

Celeste

0 项奖励
回复