Gui Guider: no widgets to select from

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Gui Guider: no widgets to select from

1,596 次查看
HansDampf
Contributor I

Dear all,

 

I am new to Gui Guider, downloaded the current version for Linux (Version: 1.8.0-GA ). I am on Ubuntu 22.04, on X86. When start a new project, with simulator target or RT1052, no widgets are shown.

 

I watched some videos about the Gui Guider, there are always the widgets on the left side. As well as in this instructions

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/Tool-Step-By-Step-Guider-of-using-GUI-Gu...

the left side of the GUI Guider is full of widgets. But not so on my installation. Is there a secret switch to enable the widgets? Or a bug on the Linux version of the 1.8.0?

 

Thanks

0 项奖励
回复
2 回复数

1,563 次查看
HansDampf
Contributor I

Hi Edwin,

thanks for the quick reply. That was the secret, found it and it works. Great.

 

0 项奖励
回复

1,574 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @HansDampf,

With the latest version of GUI Guider, the Widgets panel on the left side now shows the "placed" widgets on each screen, rather than displaying the widget list. 

Now, the widget list can be opened from the "widget" icon on the top left area below UI Editor:

EdwinHz_0-1722881771815.png

Click on it, then click the "Expand" button and you will see all of the new widget list:

EdwinHz_1-1722881866954.png

 

BR,
Edwin.