GUI guider compile error:'SDL2/SDL.h' file not found

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GUI guider compile error:'SDL2/SDL.h' file not found

6,177 次查看
richen
Contributor I

How to figure out the compile error : 'SDL2/SDL.h' file not found

Use MAC OS 12.6 and latest guy guider version.

0 项奖励
回复
5 回复数

6,164 次查看
LiubinGong
NXP Employee
NXP Employee

Hi  richen

  Is your computer architecture arm64?  In response to this problem, I suggest that you can install SDL with source code. Please ensure the install path is /usr/local.  Since the current version is not yet supported by M-core laptops, Some functions will have problems. it's predictable. BTW, We will officially support the ARM64 M-core Mac laptop in the next release(1.6.0). 

BR

Liubin

0 项奖励
回复

5,601 次查看
application_ninja
Contributor V

Any update on this? Still a problem on Gui Guider 1.6.1 with a M-Core Mac...

0 项奖励
回复

5,592 次查看
LiubinGong
NXP Employee
NXP Employee

Hi @application_ninja 

 Please install the SDL based on the steps:

Capture.PNG

Thanks

Liubin

3,524 次查看
lizm0712
Contributor I
it useful,thanks!
0 项奖励
回复

5,573 次查看
application_ninja
Contributor V

This worked, thank you!

0 项奖励
回复