GUI Guider 1.6.0 列表控件添加后无法运行,一直处于卡死的状态

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

GUI Guider 1.6.0 列表控件添加后无法运行,一直处于卡死的状态

跳至解决方案
3,018 次查看
YoungWind
Contributor III

1.如下图,添加List 控件后,点击运行程序,发现一直处于卡死的情况,这可能是个严重的问题

YoungWind_0-1693753317081.png

 

YoungWind_1-1693753397678.png

 

 

 

 

坚持做自己喜欢的事
0 项奖励
回复
1 解答
2,895 次查看
LiubinGong
NXP Employee
NXP Employee

Hi @YoungWind 

   After investigation, This is the root cause. it was found that the default font was deleted from your project. and the preset style used.  So, you can create a new project with the local project. 

By the way, we will add the missing font check for Gui Guider. Thanks for your report.

Best regards

Liubin

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,934 次查看
LiubinGong
NXP Employee
NXP Employee

Hi @YoungWind  

    I just tried to run the simulator with the same as your project. It works fine.

So would you describe it in more detail? or give a simple example project? 

Best Regards

Liubin

0 项奖励
回复
2,912 次查看
YoungWind
Contributor III

你好!

      附件是我上传的demo,我还是无法运行它(我的系统windows 11,64bit,16G运行内存),以下是我的工程配置:

1.工程配置

YoungWind_0-1693838780170.png

2.我又发现了更多的问题,添加以下控件后都无法运行

YoungWind_1-1693839173404.png

YoungWind_2-1693839253505.png

 

 

 

坚持做自己喜欢的事
0 项奖励
回复
2,896 次查看
LiubinGong
NXP Employee
NXP Employee

Hi @YoungWind 

   After investigation, This is the root cause. it was found that the default font was deleted from your project. and the preset style used.  So, you can create a new project with the local project. 

By the way, we will add the missing font check for Gui Guider. Thanks for your report.

Best regards

Liubin

0 项奖励
回复
2,870 次查看
YoungWind
Contributor III

非常感谢!确实是我删除了默认的字体导致的。

坚持做自己喜欢的事
0 项奖励
回复