GUI Guider 1.6.0 列表控件添加后无法运行,一直处于卡死的状态

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GUI Guider 1.6.0 列表控件添加后无法运行,一直处于卡死的状态

Jump to solution
3,020 Views
YoungWind
Contributor III

1.如下图,添加List 控件后,点击运行程序,发现一直处于卡死的情况,这可能是个严重的问题

YoungWind_0-1693753317081.png

 

YoungWind_1-1693753397678.png

 

 

 

 

坚持做自己喜欢的事
0 Kudos
Reply
1 Solution
2,897 Views
LiubinGong
NXP Employee
NXP Employee

Hi @YoungWind 

   After investigation, This is the root cause. it was found that the default font was deleted from your project. and the preset style used.  So, you can create a new project with the local project. 

By the way, we will add the missing font check for Gui Guider. Thanks for your report.

Best regards

Liubin

View solution in original post

0 Kudos
Reply
4 Replies
2,936 Views
LiubinGong
NXP Employee
NXP Employee

Hi @YoungWind  

    I just tried to run the simulator with the same as your project. It works fine.

So would you describe it in more detail? or give a simple example project? 

Best Regards

Liubin

0 Kudos
Reply
2,914 Views
YoungWind
Contributor III

你好!

      附件是我上传的demo,我还是无法运行它(我的系统windows 11,64bit,16G运行内存),以下是我的工程配置:

1.工程配置

YoungWind_0-1693838780170.png

2.我又发现了更多的问题,添加以下控件后都无法运行

YoungWind_1-1693839173404.png

YoungWind_2-1693839253505.png

 

 

 

坚持做自己喜欢的事
0 Kudos
Reply
2,898 Views
LiubinGong
NXP Employee
NXP Employee

Hi @YoungWind 

   After investigation, This is the root cause. it was found that the default font was deleted from your project. and the preset style used.  So, you can create a new project with the local project. 

By the way, we will add the missing font check for Gui Guider. Thanks for your report.

Best regards

Liubin

0 Kudos
Reply
2,872 Views
YoungWind
Contributor III

非常感谢!确实是我删除了默认的字体导致的。

坚持做自己喜欢的事
0 Kudos
Reply