Calling a custom Function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Calling a custom Function

1,581件の閲覧回数
sajithdevidas
Contributor III

i wrote a function inside custom.c, for the continuos movement of meter needle, how can i call the function repeatedly, i called the function in main while loop, the function is calling repeatedly but it does not shows any changes in the display, but while calling the function using timer handler its working fine, but using timer handler the function is calling with very less frequency, even i created a timer using 'lv_timer_creatre", and gave 10 ms period, then also the function is calling after 100ms only,

How can i call my custom function in while loop, is there any another methode is available?

im using rt1170evk board with gui guider

0 件の賞賛
返信
1 返信

1,534件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @sajithdevidas,

Could you please take a look at the following information?

It might be useful to look at.

Best regards, Raul.

0 件の賞賛
返信