Calling a custom Function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Calling a custom Function

1,569 Views
sajithdevidas
Contributor III

i wrote a function inside custom.c, for the continuos movement of meter needle, how can i call the function repeatedly, i called the function in main while loop, the function is calling repeatedly but it does not shows any changes in the display, but while calling the function using timer handler its working fine, but using timer handler the function is calling with very less frequency, even i created a timer using 'lv_timer_creatre", and gave 10 ms period, then also the function is calling after 100ms only,

How can i call my custom function in while loop, is there any another methode is available?

im using rt1170evk board with gui guider

0 Kudos
Reply
1 Reply

1,522 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @sajithdevidas,

Could you please take a look at the following information?

It might be useful to look at.

Best regards, Raul.

0 Kudos
Reply